(0)| 7/12/2010 11:10 AM | |
|
Posts: 77 Rating:
|
Dear All, I am getting attached herewith error while starting Runtime project on a PC where only Runtime software is installed. I have also installed required licenses. Please guide why it is happening. Error report is attached herewith. Thanks & Regards,, Attachment1.pdf (747 Downloads) |
| 7/12/2010 1:51 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC? Best regards, Hristo Mihalev |
| 7/13/2010 9:03 AM | |
|
Posts: 77 Rating:
|
Dear UMENCHO, Thanks for your reply. I have followed the steps in the FAQ. But I am still not getting the results, I am getting some error of .ini file which is shown in the file attached. As mentioned in the FAQ, I have done as follow: 1. Copy the Runtime file "*.fwx" into the folder that specified in the RT Loader under "Settings > Directories > Configuration file". 2. Change the name of the file from "*.fwx" to "PDATA.fwx". Example: Project_RT_01.Panel_1.fwx => PDATA.fwx I am doing the manual configuration instead of using Transfer Function mentioned. Please suggest, Thanks & Regards,, Attachment2.pdf (450 Downloads) |
Last edited by: S7Mgr at: 7/13/2010 9:06 AM |
|
| 7/13/2010 1:32 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
So, seems with changes that made you need to change also ini file. Select configuration file Open the folder in which the configuration file "HmiRTm.ini" is located. In a standard installation, this is the path "C:\Program Files\Siemens\SIMATIC WinCC flexible\WinCC flexible 200x Runtime\"(the path might be slightly different depending on the language version of the operating system installed). Edit configuration file Right-click on the "HmiRTm.ini" file and open it via the menu item "Open". Enter the copied path and then save the file. Example: Note: Try to execute and follow http://support.automation.siemens.com/WW/view/en/32813726 But the question is still there - What exactly did you did and for this reason you went in troubles... Hope this helps. Best regards, Hristo Mihalev |
| 7/14/2010 7:26 AM | |
|
Posts: 77 Rating:
|
|
| 7/14/2010 12:19 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Thank you for feedback. Perhaps in future Service Pack 2 for SIMATIC WinCC flexible 2008 also will helps you. Best regards, Hristo Mihalev |
Follow us on