(0)| 8/11/2010 7:24 AM | |
|
Posts: 3 Rating:
|
Hi ! As a novice in using AI/AO modules on S7, I tried to connect an device that gives 4-20 mA to a AI module 6ES7-331 7KF00-0AB0. Reading the getting started manual I decided to use 2-wire connection ( type of measurement 2DMU). There is a problem in measuring, because I am not sure if I could use 4-wire connection, and how could I konw which wiring principle is better ?! The HACH-LANGE SC100 controler provides me with 4-20 mA, and I can measure them, but the reading on my AI module is always the same ?! Is it posible to configur AI module when the PLC is in run mode ( I sould not stop the proccess)? Please if there is someone who has more experience with the AI configuration to give me an advice. Kind regards, Marko. Splitted from problem with sm 331 8*12 AI. |
Last edited by: O_Moderator at: 8/11/2010 11:06 AMnew subject after splitting |
|
Follow us on