(0)| 8/18/2010 4:44 AM | |
|
Joined: 10/7/2005 Last visit: 1/22/2026 Posts: 3054 Rating:
|
Hello Glenn Merrell, CAP here's one way: 1.) Find a free (not yet used) FB 2.) Find a free (not yet used)Timer 2.) Add the example logic below to the FB (adjust time delay value to suit) 3.) Call the FB from OB22 Example Logic: A F 255.0 // Scratchflag ANF 255.0 // Create RLO of 0 LKT 010.2 // 10 seconds delay SD T 77 //Call On delay timer with RLO of 0 (i.e.initialise Timer) O F 255.0 // Scratchflag ONF 255.0 // Create RLO of1 SD T 77 //Call On delay timer with RLO of 1 (i.e. start Timer) LOOP:ANT 77 // Timer still running? JC=LOOP // --> wait in Loop BE I hope this helps |
|
Cheers |
|
| 8/18/2010 5:47 AM | |
|
Posts: 3 Rating:
|
Tank Fritz! |
This contribution was helpful to
|
|
Follow us on