(1)| 6/10/2010 4:46 AM | |
|
Posts: 26 Rating:
|
Hi All, Can I connect OP277 to CPU 95U through CP541-L2? I have browsed in this forum anything about CP541 but i found no answer. Please help, Saptauto |
| 6/10/2010 3:39 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello Saptauto, I have manual of CP541. Look at attachment. OP277 is possible to connect to Step5 via Profibus DP protocol. best regards, Hristo Mihalev Attachment6ES5 998-1DL21.pdf (428 Downloads) |
| 6/10/2010 10:15 PM | |
|
Joined: 10/7/2005 Last visit: 1/22/2026 Posts: 3054 Rating:
|
I'm afraid you can NOT dear saptauto. While the the CP541 is a SINEC L1 to Profibus DP (well SINEC L2 to be precise) converter, your PLC would need to be a DP Master and you woudl need tobe able to configure the Panel as a DP Slave for ti via the CP541 to make it work (which you can NOTdo with the SINEC L1 port). Having said that, should you have a 95U with an onboard DP Master port (part number 6ES5 095-8ME02) you can connect the OP277 to it (without the need fora CP541). Note too that Siemens has just relaesed SP2 for WinCC flexible 2008 and "ressurected" support for AS511 communications. This means that you can now again use the AS511 programming port of your S5 to connectcertain HMI Panels. I hope this helps |
|
Cheers |
|
This contribution was helpful to
|
|
| 8/23/2010 9:53 AM | |
|
Joined: 10/7/2005 Last visit: 1/22/2026 Posts: 3054 Rating:
|
Hello saptauto I somehow managed to miss you previous follow up question (apologies for that), as luck would have it, another user just asked the same qeustion andI hope the answer to THIS thread will help you too. |
|
Cheers |
|
| 8/23/2010 11:13 AM | |
|
Posts: 26 Rating:
|
Dear Fritz...... Thank you very much..... |
This contribution was helpful to
|
|
Follow us on