(0)| 8/24/2010 4:56 PM | |
|
Posts: 4 Rating:
|
Dear All: I need your help about loading from the hard drive. We are following the procedure to load TEA files, but we keep getting error at Step 56, which is to load TEA 3 file from Drives Drive MD ==> Load From Disk ==> Set "Config" ==> Accept Conf + NCK PO ==> File Function ==> Load From Disk ==> Set "Drives" We keep getting the same error at this step: 165005 Error in Data Transfer There are two more errors that pop out from the screen as well: they are "9296 CNC Alarm", and " 1280 ORD7 X Measuring Circuit Not Available" These two errors were nowhere to be found in the manual. Can you point me to the direction to fix these errors? Best Regards, SurfengLee Attachment840C Reload from hard drive.pdf (365 Downloads) |
| 8/26/2010 5:47 PM | |
|
Posts: 4 Rating:
|
Does anyone know what "9296 CNC Alarm" means? |
| 8/27/2010 8:19 AM | |
|
Joined: 1/19/2008 Last visit: 10/20/2025 Posts: 998 Rating:
|
Four digit alarm numbers from 9000 upwards are generated by whoever wrote the plc. |
Follow us on