8/27/2010 6:54 PM | |
Joined: 3/28/2010 Last visit: 9/17/2025 Posts: 1172 Rating:
|
What materials of construction are used for the piping ? |
8/30/2010 3:52 AM | |
Posts: 23 Rating:
|
The material of pipe is SS 316L. |
9/1/2010 3:57 AM | |
Joined: 3/28/2010 Last visit: 9/17/2025 Posts: 1172 Rating:
|
See attached pages for material properties of Hastelly C276, Monel and Tantalum. Pages from Handbook of Corrosion Engineering by Pierre R. Roberge McGraw-Hill, 1999, ISBN 0-07-076516-2 Attachmentpage 687 (111) Monel 400 properties.pdf (290 Downloads) |
9/1/2010 3:59 AM | |
Joined: 3/28/2010 Last visit: 9/17/2025 Posts: 1172 Rating:
|
see attachment
Attachmentpage 682 (106) Hastelloy C276 properties.pdf (315 Downloads) |
9/1/2010 4:01 AM | |
Joined: 3/28/2010 Last visit: 9/17/2025 Posts: 1172 Rating:
|
see attachment (no means to upload multiple attachments, grrrrrr . . . . .)
Attachmentpages 703-707 (127-131) Tantalum properties.pdf (326 Downloads) |
9/6/2010 4:36 AM | |
Posts: 23 Rating:
|
How about if I choose SS316 with PTFE coating for this? With pressure up to 6 bar and temperature <100 and the others >100 C. Degree. And one more problem: the pressure transmitter will be installed on pipe with the smallest diameter 38mm. Which process connection can be used in this case? And we attach the detailed specification. Please advise us. Attachment00.Spec.Pressure Transmitter list.pdf (324 Downloads) |
Follow us on