9/8/2010 8:21 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, You could use either Parameter List: MICROMASTER 420, either Operating Instructions: MICROMASTER 420 0,12 kW - 11 kW. There have explanation about hardware connection and settings of parameters into the drive. Take a look also at MM420: start a motor with digital input Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
Follow us on