(0)| 10/2/2010 5:18 PM | |
|
Posts: 1 Rating:
|
Dear, I have a problem with the assignments of buttons in wincc flex advanced 2007. the 3 buttons on the right lower side do not response. I assigned on every button another screen . only when I select the left lower button, then the buttons on the right lower side are working. Is this a software problem? Best regards, Lieven Morlion. Splitted from Graphic list update after loss communication. |
Last edited by: O_Moderator at: 10/4/2010 1:16 PMnew subject after splitting Last edited by: O_Moderator at: 10/3/2010 10:31 AMcontact data deleted |
|
| 10/4/2010 10:26 PM | |
|
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Hi, That sounds kind of unlikely. Have you checked the properties of the rightbuttons to make sure that they are not relatedto the one on the left? 1. Create a new program from scratch 2 Program only one of the right buttons and try it. Regards, Behnam CPU315 <-> S120, How????? |
Follow us on