10/24/2010 1:07 PM | |
Posts: 14 Rating:
|
Sir, We are using CuVC & CU-1 type drives for our operations. But when i try to take parameter backup of all the drives with drive monitor, i am abloe to take the backup of CuVC drives only. Whenever i connect my FC drives, then device identification error comes which says -- "your device is not recognized." In that it shows that current device version is 1.2 and configured deviceversion is 1.3. But in drive monitor when i selectmy Drive type, i select Simovert FC then only one version is displayed which is 1.3 and 1.2 is not shown, so i select 1.3 and when i press ok,the above error comes.However, i noticed that if i select Cu-2 type drive then version 1.2 is displayed. Thou i don't select that. So, how should i proceed to take the backup of my FC drives coz neither SIMOVIS nor Drive Monitor is identifyingthe drive. Pls help me ASAP. Thanks & Regards V@Bz...... |
10/27/2010 6:46 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Make offline file... Select version whatever shows in your drive monitor.. Click on online button (Write EEPROM button) You will get Firmware mismatch error but you will be able to take backup and even download same.. Check out following Discussion https://www.automation.siemens.com/tf/WW/en/Posts/44920 Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on