11/9/2010 4:24 PM | |
Posts: 739 Rating:
|
Hi, as first: be carefully with the data sets of the AOP. If you need to store one data set, you have to delete one language first! If this language is deleted you do not have any chance to restore it! If every language is deleted you can trash your AOP. For further information please see this cluster: http://support.automation.siemens.com/WW/view/en/26435762 |
11/9/2010 11:36 PM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi Pavel, I think you need to change the AOP mode to Slave, this way, you can access the internal AOP parameter set and the current drive parameter set. Then you can access each stored parameter set as a USS address from 00 - 09. See the attached manual Hope this helps, Cheers, Graeme
AttachmentAOPEnglish.pdf (261 Downloads) |
Follow us on