11/17/2010 11:28 PM | |
Posts: 1 Rating:
|
Estimates I wish to know to do, is that I have a frequency vector control SIMOVERT MASTERDRIVES AFE, the process begins when energized works normally but when I placed the maximum speed the drive sends me over voltage to DC and who is the inverter that makes the drive stops and the main switch is open. In another instant the rectifier process opens sending a Surge in DC and this causes the PLC to lose communication and opens the main switch, this will program the drive so it can withstand the maximum continuous DC voltage. But with all the main switch is opened. Any suggestions or support for this case. Splitted from Servo motor query. |
Last edited by: O_Moderator at: 11/19/2010 1:03 PMnew subject after splitting |
|
Follow us on