(0)| 11/7/2010 4:03 PM | |
|
Posts: 1742 Rating:
|
Hello, The block seems to come from the libary "RLG" (Regelung in German)which contains the blocks for PID controllers. The FB you show us seems to realize a step controllerwith two outputs (with heating and cooling outputs) In S7-300 you can realize PID controllers using S7 system functions described in this manual http://support.automation.siemens.com/WW/view/en/44240604 See chapter 28 You will have to replace the FB232 with the equivalent blocs of the S7-300 I believe it is bettre to postconversion issues in the conference "Simatic S5") where ofmost conversion issues are posted (to get a faster answer). |
| 12/4/2010 4:44 AM | |
|
Posts: 24 Rating:
|
If i not mistaken this is standard block and i'm not so sure what number it is..still in trouble with that.. arghhh..!!i can't solve bro..please help me...
|
Follow us on