(0)| 12/20/2010 11:46 AM | |
|
Posts: 316 Rating:
|
Hi Shar, you can use the Vision like ossaexplaned in this Thread (first answer). With the vision you can set or reset the bits. "Read" the bit. tbXX := tINT.b04; Set or Reset the bit. tINT.b04:=TRUE; OR tINT.b04:=FALSE; If you want to change more than one bit, you can build up the AT vision as an array of byte. Then you have a dynamic acess possibility on the bits. |
| 12/20/2010 1:50 PM | |
|
Posts: 316 Rating:
|
Hi, the thread were splitted... so my reference is lost in this thread. The reference you will find on the following link: /tf/WW/en/Posts/47335#top Ossa wirtes: do this .... VAR_TEMP tiINT : INT; //Integer value EN_VAR . BEGIN tiINT := <whatever integer your are looking at>; tbXX := tINT.b04; //Fetch bit 04 in the integer |
Follow us on