(0)| 1/19/2011 6:43 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello ragnarok; You could use the WinCC Flexible OPC connections, setup the panel as a OPC server, and create (or dowload code for) am OPC client for your VB application: SIMATIC HMI WinCC flexible 2008 Communication Part 1: http://support.automation.siemens.com/WW/view/en/18797552 To communicate using the OPC communication driver, WinCC flexible has a suitable COM interface over which data can be exchanged between automation systems. An HMI device can be used either as an OPC server or OPC client. As an OPC client, the HMI device can connect to a maximum of 8 OPC servers. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/19/2011 6:44 PM |
|
Follow us on