(0)| 3/4/2011 2:45 PM | |
|
Joined: 10/7/2005 Last visit: 1/19/2026 Posts: 3054 Rating:
|
Hello RandomCoder you need to set the restart mode to "Hot Restart" (which means OB101 is used) in the "Startup" tab of the CPU properties if you want to retain the process image (you can additonally select to "reset the outputs at Hot restart" or deselect this option too). Note thatthe program will in this mdoe resume at the point in the program where if stopped when the power failed. Please make sure to use the "Help" button on the "Startup" tab of the CPU propertiesand read up on the rarifications of this mode. I hope this helps |
|
Cheers |
|
Follow us on