(0)| 3/30/2011 6:36 AM | |
|
Posts: 9 Rating:
|
Can we use 2 BLM-objects in 1 CU ? Is this configuration is allowed to load into the CU320 or there is any software restrictions in the system ? In our system, there two BLMs whose DC bus is common feeding to one Momo ? We do not want to configure as parallel configuration.... AttachmentDrive connections.pdf (323 Downloads) |
| 3/30/2011 4:09 PM | |
|
Posts: 133 Rating:
|
Only one independant Line Module can be connected over Drive CLiQ to a CU320 or CU320-2 |
Follow us on