(0)| 5/16/2011 3:44 AM | |
|
Joined: 10/7/2005 Last visit: 1/22/2026 Posts: 3054 Rating:
|
Hello cantona a simple search for "CIR" at https://support.automation.siemens.comreveals a number of FAQ's and procedures, all that's left for you is to pick the one that suits your system (you'll also be able to find a fair few Forum related discussions about this topic): SIMATIC STEP7 V5.5 Modifying the System during Operation via CiR SIMATIC STEP 7 V5.4 Modifying the System during Operation via CiR Which DP slaves can be added to and removed from a PROFIBUS DP master system using the CiR function (Configuration in RUN) and which configuration changes are permissible? What should you watch out for when adding components or changing their parameters using CiR (Configuration in Run)? Which are the hardware requirements for CiR (Configuration in Run) at SIMATIC PCS 7 V6? What should you watch out for when using the "Configuration in Run" (CiR) function on the PROFINET IO system?(unlikely to be aplicable as you seem to use PCS7) I hope this helps (and if not, please provide us with more detail as Ammyalready suggested) |
|
Cheers |
|
| 5/17/2011 3:21 PM | |
|
Posts: 5 Rating:
|
thank u all it was helpful |
This contribution was helpful to
|
|
Follow us on