(0)| 5/8/2011 4:52 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Perhpas there you will find an answer- http://support.automation.siemens.com/WW/view/en/837001 http://support.automation.siemens.com/WW/view/en/18645578 Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 5/8/2011 4:54 PM |
|
| 5/11/2011 11:33 AM | |
|
Posts: 204 Rating:
|
Thanks for yours help, I found what I need |
| 5/24/2011 10:50 AM | |
|
Posts: 1121 Rating:
|
Hi Note that if you have a DB and try to download full program or the DB alone the value in the db that was stored shall change to intial value. Have fun.. |
| 5/24/2011 12:20 PM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Hi Cells in a datablock can be considered as 1- The read only cells in which, you only read the data.These are possibly the constant or some scientific coeficient which is used in calculation.They are initialized and the values be unchanged for a long time. 2-The other cells, the CPU can write in them and they may change simply after you downlad the project.It is always a matter of problem.In process with adaptive parameters or process with lots of modification of setpoints and controllers' parameters, it is recommended to update the finalized DB values after finishing commissioning or before downloading the raw and original program.This is an important fact "The machine or process stabilized by the Values of datablock inside the CPU". Also check the following post: Datablock backup
Regards |
Follow us on