(0)| 5/25/2011 1:48 PM | |
|
Posts: 7 Rating:
|
Hello for all, I have problem with cp343-1 lean, version in project is V2.2, but I can't see and I don't have this version in HW catalog. I try to install hardware updates (download from internet, found 1043 and download it). I can't install 1043 after, because cp343-1 still missing in list. Have someone had same problem and how to solve. Current version of step 7 is S7 SP5 HF1. Thank you all in advance, Dusan. Attachmentcp343-1v2.2.zip (340 Downloads) |
| 5/25/2011 2:10 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, |
| 5/26/2011 4:01 PM | |
|
Posts: 947 Rating:
|
Hi! With update V2.3, the CP 343-1 Lean (6GK7343-1CX10-0XE0) is functionally compatible with the predecessor version. It can therefore be configured with the same STEP 7/NCM version (configured as in the past as a CP 343-1 Lean (CX10) with V1.0/V2.0/V2.1/V2.2). It is not necessary to upgrade STEP 7 or NCM when using the compatible functions. |
Last edited by: gre_m at: 5/26/2011 4:02 PM |
|
| 6/1/2011 9:21 AM |
|
|
Posts: 1121 Rating:
|
Hi Dirdule, Thank you for posting your feedback, Have fun... |
Follow us on