(1)| 6/6/2011 12:07 PM | |
|
Posts: 103 Rating:
|
HI EVERYONE what is the benefit to unlink the db and how it is possible thanks |
| 6/6/2011 12:12 PM | |
|
Posts: 691 Rating:
|
May be this thread will help you https://www.automation.siemens.com/tf/WW/en/Posts/45535 |
| 6/7/2011 8:22 AM | |
|
Joined: 10/7/2005 Last visit: 1/18/2026 Posts: 3054 Rating:
|
Both can be used (SFC20 OR SFC83)and apart from the link thatdchartier listedin the threadthat Sharrefered too, the following may prove useful too: How can the program runtime be optimized if the main memory of the CPU is too small for the runtime-relevant STEP 7 program?" |
Last edited by: fritz at: 6/7/2011 8:25 AMCheers |
|
| 6/7/2011 8:29 AM | |
|
Posts: 1750 Rating:
|
Both can be used (SFC20 OR SFC83)and apart from the link thatdchartier listedin the threadthat Sharrefered too, the following may prove useful too: How can the program runtime be optimized if the main memory of the CPU is too small for the runtime-relevant STEP 7 program?" Dera fritz Thanks for confirming that SFC20 can be used. i got confused for a while. Now it is clear that both SFC can be used. |
Follow us on