7/17/2011 11:11 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, Have a look to this manual, chapter 6. http://support.automation.siemens.com/WW/view/en/37436836 To have the best performance,I suggest togroup all the data to be visualized in only a few DBs. To avoid too much mutiple requests to gather the required data. In thethe latest models of CP1430TF and CP1430 TCP, both AUI and ITP are implemented in the SINEC H1 connector of the CP. To connect a CP1430 TF or CP1430 TCPusing ITP (ITP= industrial twisted pair), there isan ITP convertercable ended on one side with 15 pin, the other side with RJ45 (see http://support.automation.siemens.com/WW/view/en/27706734) |
Best regards |
|
Follow us on