(1)| 7/17/2011 1:19 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello Tumati; The following link will open the operation instructions manual for the Sitrans F Mag 6000 flowmeter Modbus RTU module. http://support.automation.siemens.com/WW/view/en/44880906 Appendix A contains the Modbus mapping for the Mag 6000, listing all parameters available, their Modbus address and datatype. Chapter 6 explains which Modbus Functions are supported by the module, and what datatypes each of these Modbus Functions can transmit. Hope this helps, Daniel Chartier |
Follow us on