(0)| 8/16/2011 9:04 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Joined: 5/28/2008 Last visit: 1/12/2026 Posts: 4522 Rating:
|
Hello,
Now let us calculate what is the required resolution for achieving 0.01mA precision. +27648 = +20 mA 0 = 4mA Each 1 unit = 1*slope = 1*[(20-4)/(27648-0)] = (16/27648) = 0.00058 mA. And according to the following table:
For 8 bit resolution module => Min units = 128, res. =0.00058 * 128 = 0.07424 mA For 9 bit resolution module => Min units = 64, res. =0.00058 * 64 = 0.03712 mA . . For 15 bit resolution module => Min units = 1, res. =0.00058 * 1 = 0.00058 mA Hopethis helps.
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Ayman Elotaify |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Follow us on