(0)| 8/25/2011 4:11 PM | |
|
Posts: 6 Rating:
|
Hey folks, I'm just starting to dig into this project and it's been years since I've worked with Siemens. The production line I'm working on is fairly old and quirky. I thought I'd check the firmware version and it looks like it may be pre v2.0 but I'm not sure. I've found this link http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=16750732&caller=viewand I think I understand it for the most part. When I try and display the firmware version as shown in that link, I get no firmware version and it looks like the hardware is Version 1. Step7 V5.5 gave a message that that module (6ES7 315-2AF02-0AB0) does not support firmware updates. I see that the firmware update process requires a 4Mb memory card and I've got a 64Kb installed. Is this cpu too old to update? Software Step7 v5.5 CPU 315-2 DP #6ES7 315-2AF02-0AB0 Memory MC95/64kb/5V Flash #6ES7 951 0KF00-0AA0 |
Last edited by: Clegg at: 8/25/2011 5:08 PM |
|
| 8/26/2011 8:37 AM | |
|
Posts: 27 Rating:
|
Hey Clegg I think this cpu is to old for a update. look at this link: http://support.automation.siemens.com/WW/view/en/26290163 |
Follow us on