(0)| 8/29/2011 3:32 PM | |
|
Posts: 65 Rating:
|
Hi I'm about to change CPu from 318 to 319 and when i started to replace the CPU it changes the ID in the Netpro From 0001 A050( CPU318)to 0001 A020 (CPU 319). Try ty change it but i cant. This CPu are connected to more Cpu's and other forms och cummunication/networks. My question is i have to change the id in the other projektmanager's for the communication partners? (Local ID and partner ID). Or how to change back from 0001 A020 to 0001 A050. Att. an screen dump fore som more info. If i don't can change the local ID, do i have to change in every station och download netpro?. ( i guess it's so). So the best is if i can change back the local ID, but it mabey is related to the CPU.? Were from come's that local ID in netpro, is it something the modul is making or is it changeable? AttachmentID.zip (145 Downloads) |
Last edited by: NickeNyfiken at: 8/30/2011 7:35 AMLast edited by: NickeNyfiken at: 8/29/2011 4:35 PMLast edited by: NickeNyfiken at: 8/29/2011 4:34 PM |
|
| 8/31/2011 7:37 AM | |
|
Posts: 2348 Rating:
|
Can you upload HW here? I mean original one with CPU318 - i can try to change it. And please specify CPU319 order number. |
| 8/31/2011 10:44 AM | |
|
Posts: 65 Rating:
|
It's to big to upload, will try to make it smaller.
|
| 8/31/2011 1:21 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Contact with Moderator in order to help you for that. Best regards, Hristo Mihalev |
| 9/2/2011 11:37 AM | |
|
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Attached is the file sent to me by NickeNyfiken. Best regards O_Moderator AttachmentS7-linje.zip (135 Downloads) |
| 9/2/2011 5:13 PM | |
|
Posts: 1121 Rating:
|
HI well can you give us the MLFB of CPU319 have fun... |
Follow us on