(0)| 9/7/2011 7:44 PM | |
|
Posts: 4 Rating:
|
Hello Guys! I have a similary problem with timers. Let me explain what is my problem. I have two timers T1 and T2, When i detect a metal the M8.0 memory will addressed and start the T1 Timer. T1 counts 2sec after 2sec on the out T1 will adderss the M8.1 what is the activation for T2. T2 will count 4 sec. and this is one cycle. T1+T2= 6sec I need to make that when i detected the metal the counter will start to work, but if the transporter stops working i want to pause the counting. and when the transporter start to work counter will start do count down wher it was paused. If it was stopt on 3 sec that means the T2 will start from 3.1 sec till 4 sec. Sorry fir my bad english and i hhope that my explanation is clear. Thanx, and best regards Splitted from Can i pause timers or program. |
Last edited by: O_Moderator at: 9/8/2011 8:59 AMnew subject after splitting |
|
| 9/8/2011 9:42 AM | |
|
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread Siemens S7 300 Timer problem solwing. Best regards O_Moderator |
Follow us on