(0)| 9/12/2011 2:33 PM | |
|
Posts: 376 Rating:
|
Hello majoza1, I think thecause for the problem can beonly a wrong attitude for the EPROM driver. Here some information from the manual COM PROFIBUS. You find the manual COM PROFIBUS here: http://support.automation.siemens.com/WW/view/en/1498610 If you use the manual in English, please use the function “Download”. Chapter 2 Installation and uninstallation. The following about the Installing COM PROFIBUS. In the manual SIMATIC COM PROFIBUS on page 13 find you the following information. On memory card parameterization. During installation, a program for parameterize the memory card is also installed. After installing COM PROFIBUS, you can start this program as follows from the Windows Start menu: Start > Programs > Siemens COM PROFIBUS > Memory CardParameter Assignment Possible settings:· If you are not using an EPROM driver, select the "No EPROM Driver" option. Please check this setting "No EPROM Driver". · Otherwise, select the appropriate entry for your programming device. · If you are using a PC, you can select a driver for an external PROMprogrammer. You must also specify the interface (e.g. LPT1) to which thePROM programmer is connected. More information find you in the chapter 7 and 8. In chapter 7 Importing configurations you find information about the function “Importing data from a memory card". In chapter 8 Exporting configurations you find information about the function “Exporting data to a memory card". I hope this information helps you. Best Regards Azteke0110 |
| 9/12/2011 4:16 PM | |
|
Posts: 4 Rating:
|
My problem: i have in my project config. wibond (ET200U 6ES5 318-8MB11) GSD file SI8002UX.200 (see attachment). I don't export this project in comprob v3.1 to mem. card, probably my PG with OS xp is not correct working with this comprofibus v3.1. I know It not possible configured this module in comprofibus v 5.1. somebody knows how to configured this module in comprofibus v.5.1 ? I must replaced this module with another, when i want config. in compb. v5.1? Attachment185388.zip (453 Downloads) |
| 9/13/2011 12:50 PM | |
|
Joined: 8/25/2006 Last visit: 1/19/2026 Posts: 2221 Rating:
|
Hello. To configure ET200U in ComProfibus V5.1 install GSD-file from here(copy it to the C:\Siemens\CPBV51\gsd). To open your project without errors you need to copy SI8002UX.200 file from ComProfibus V3.x folder to the C:\Siemens\CPBV51\typdat5x. |
| 9/14/2011 12:42 PM | |
|
Posts: 4 Rating:
|
Hi, I try this as fisrt step when i open my project in v5.1 but this module (SI8002UX.200) is in GSD files with errors see attachment. |
Follow us on