(1)| 10/7/2011 11:11 AM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Dear saeedplc, The M-memory will be zero, when the CPU starts. (Or when they are retentive, they will have the value when power fails) A Datablock can contain memory area's with an initial value (start value) One example of using Datablock, could be recipe values. Perhaps this link might help: What is the significance or the initial and actual values of a data block? What does the terms Initial value (declaration view), Initial value (load memory) and Actual value mean in data blocks when a controller is loaded / restarted? how can you back up the actual values of DBs and bit memories? Best regards, Wizard |
Follow us on