(0)| 10/28/2011 2:06 PM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Dear Chris.Percival, Please check the following codes as a sample to access parameters declared as UDT in input and output of a function. Attachment contains the whole project. [code] TYPE "HDUDT" VERSION : 0.1 STRUCT ONE : DWORD ; TWO : DWORD ; END_STRUCT ; END_TYPE[/code] [code]FUNCTION "HDFC1" : VOID TITLE = VERSION : 0.1 VAR_INPUT HDFCE : "HDUDT"; END_VAR VAR_OUTPUT OUT1 : BOOL ; HDFCA : "HDUDT"; END_VAR BEGIN //CODE START NETWORK TITLE = L #HDFCE.ONE; L #HDFCE.TWO; ==D ; = #OUT1; ///////////////copy////////////////// L #HDFCE.ONE; T #HDFCA.ONE; L #HDFCE.TWO; T #HDFCA.TWO; END_FUNCTION[/code] Best regards AttachmentUDT_FC.zip (143 Downloads) |
Follow us on