(0)| 11/1/2011 10:05 PM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Dear carahigo, As I may understood your requirements, you want to have 16-bit memory area in CPU which can be bit-wise accessible (read and write access) and the whole 16 bit can be addressed as a WORD or INT for easier transfer to HMI.If my assumptions were right, so a memory word may help you to do the task.For example MW0 is set of 16 bits from M0.0 to M1.7 which can be accessed individually( with their own symbol) or as a whole. Also possible to implement this idea in data blocks.To do so check the solution in attached project. Best regards, Hamid Hosseini Attachmenttest2.zip (142 Downloads) |
Follow us on