(0)| 1/7/2012 1:12 PM | |
|
Joined: 10/7/2005 Last visit: 1/19/2026 Posts: 3054 Rating:
|
Hello The_beginer I'm afraid to say that neither Network is correct as either will detect a0 to 1 transition of M28.6. If you however change the --(P)-- to an --(N)-- instruction, then both will do the job, in which case though I would use the logic in NW 5 (the extra move in NW 6 is wasteful and achieves nothing). One more thing, make sure to have MD26 as part of the retentive M area (declared inCPU properties) if you need it to retain its value after a CPU restartor use a DBD alternatively. I hope this helps. |
|
Cheers |
|
Follow us on