(0)| 1/22/2012 6:58 PM | |
|
Posts: 21 Rating:
|
I would kindly ask an HELP understanding why the TIMER do NOT be RESTART after the FIRST Time. Basically, in the attached example, I need a time delay each time a record is transfered to the HMI. The start signial is given by a memory variable in the FB, that I SET each time needed, and clear each time the Timer elapse. But it works only the first time. I tried to check with PLC Sim, but without success... The key networks in the attanchements are the follows : [code]TITLE = NTWRK 5 - Set Start input for timer to TRUE AN #ST_HMI_WAIT; = #ST_HMI_WAIT; NETWORK TITLE = NTWRK 6 - time load in pulse and start // set time to wait for hmi A #ST_HMI_WAIT; L S5T#20MS; SP "ST_HMI_Timer"; NETWORK[/code] Where am I wrong ? Any help will be appreciated :-) AttachmentFB1.AWL.zip (206 Downloads) |
Follow us on