(0)| 1/27/2012 10:55 AM | |
|
Posts: 48 Rating:
|
how to determine what will be the maximum IO modules and FC, FB and DB that a particular CPU can support? |
| 1/27/2012 11:02 AM | |
|
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, It's all in the manual i linked to. For example 312 CPU see attachment. Regards, Marcjan Attachments7300_cpudata-example.pdf (404 Downloads) |
|
Problem solved? |
|
| 1/28/2012 7:25 AM | |
|
Posts: 48 Rating:
|
Is it possible to determine the work memory even before we start programming? So that we can decide which CPU is to be selected? |
| 1/28/2012 3:36 PM | |
|
Posts: 1121 Rating:
|
Hi well you can not start the FC no with "0", see the default size of the FC or a FB is 38 bytes, Before starting the programming, the user can only guess the size of the program can be. Then again depends upon the user programming skills and the number of logics that is written Normally if you write the program using the STL then the block size is less than writing the same logic with Lad or FBD. for calculating the rough estimate use the follwoing link. See the attached link for further calculation link1 Have fun... |
| 1/28/2012 5:05 PM | |
|
Joined: 8/31/2010 Last visit: 12/6/2025 Posts: 1525 Rating:
|
Hello Tagolover, Good Idea. Still in this method, you need to create the program blocks and then only check the work memory and load memory consumption. It's not possible to determine before creating
Hello pachu, Though it's an easy question (i like this question), the answer is not that easy and straight. It depends on many factors as Tagolover said, - Programmer skill - Programmer's way of thinking - Programming Language used - etc, etc Anyhow you can check with your local Siemens office / representative on the S7 family selection (S7-1200 / S7-300 / S7-400) or for CPU selection. They may give a better idea based on your application as they deal with variety of applications. |
Last edited by: Ganes10 at: 1/28/2012 5:06 PMLike it? Rate it! |
|
Follow us on