(0)| 2/3/2012 1:15 PM | |
|
Posts: 8 Rating:
|
I am working on a Siprotec device 7SD533. my problem is that Digsi refuses to load my relay parameters. Yesterday I loaded parameters to the device via the ethernet connection. Today i make changes to the IEC 61850 station and load the parameters then it gives me the errors below I have checked for all the errors nothing seems to be wrong. Unable to connect to device! Possible causes: 1. The connecting cable is not plugged into the correct PC port 2. The connecting cable is not connected to the correct device. 3. The device has not yet been initialized. 4. Parity or stop bits do not match (with RS232/RS485). 5. The IP address is not correct (with PPP/Ethernet). Attachmenterror.zip (424 Downloads) |
Last edited by: Stixx at: 2/3/2012 1:44 PMLast edited by: O_Moderator at: 2/3/2012 1:23 PMnew subject after splitting from /tf/WW/en/Posts/65717#top |
|
| 2/6/2012 6:50 AM | |
|
Posts: 8 Rating:
|
Thanks I found the problem. I did not assign an IP address for DIGSI. Problem solved |
This contribution was helpful to
|
|
Follow us on