(1)| 2/1/2009 8:44 PM | |
|
Posts: 19 Rating:
|
Hi! Can somebody help me to understand TSAP? As there is help to find on internet I must make it harder then it really is! Please see attached files, I beleave it is self explaining. I want three PLC to comminicate with each other and all to PC-Access using TCP/IP. Hopes for some good answers Dan AttachmentData Exchange.zip (2732 Downloads) |
| 2/6/2009 1:30 PM | |
|
Posts: 5822 Rating:
|
Hello, well, if I read the S7-200 PC Access V1.0 Help Systemthan I find in the chapter Ethernet Communication the information I mapped to this post as PDF.It shows you the way to go. If you want a Sample with PPI, check the Micro Automation: Simplest possible access to PLC data via standard PC applications (MAS 11) I hope this will show you the way. Best regards J_Bell AttachmentPC_Acces_Ethernet_Link.pdf (3040 Downloads) |
This contribution was helpful to
|
|
| 2/6/2012 1:25 PM | |
|
Joined: 3/21/2006 Last visit: 1/22/2026 Posts: 10248 Rating:
|
Hello,
I also want to Know that if i Configure only 1 Connection while i use Ethernet wizard, to how many HMI panels can i communicate? and how??
What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options? You should specify the type of HMI panel, taken in account
and Which HMI components can you connect with S7-200 CPU and what should you watch out for when doing so? Best regards, Hristo Mihalev |
Follow us on