2/7/2012 1:38 PM | |
Posts: 267 Rating:
|
Hello! "- What does it mean "PER"? - What does "PER" stand for?" PER=PERiphery (it's an analog valve from your process valve sensor respectively for your actuator) "- I need a simple temperature regulation, input temperature sensor 4-20mA, output regulation valve 0-10V. The user will be able to modify PID parameters like Proportional gain, Integral time, Derivative time by the means of a Touch Panel HMI. But I can't see any way to connect HMI parameters with actual PID parameters, using a DB. How to do it? I see that I can access to the PID internal DB data (i.e. "PID_Cooling".sRet.r_Ctrl_Gain, "PID_Cooling".sRet.r_Ctrl_Td, "PID_Cooling".sRet.r_Ctrl_Ti). But is it possibile to modify those parameter from outside (HMI)?" Yes, it is possible. You need a analog input signal modul or signal board to calculate your temperature sensor current to the analog value. http://support.automation.siemens.com/WW/view/en/36932465 A.6.1/A.9.1 To modifyPID parameter create an I/O field onthe screen in your HMI which accesses to the parameter in the PID instance DB.You can see which parameter is accessable by the column "Visible in HMI". "- What should be the suitable PID mudule for my application? When to use the PID_Compact, when to use the PID_3Step?" I would prefer the PID_Compact. PID_3Step is for digital valve controlling (open, close, stand still). "- Where cound I find a PID user guide ?" the same link; chapter 9.2 or the online help in STEP 7 V11 |
2/7/2012 7:25 PM | |
Posts: 57 Rating:
|
Thank you so much for your fast and kind answer. So, if I correct understand: - Better to use the PID_compact with an analog regulation valve (0-10v control). - Better to use the PID_3step with a digital regulation valve (open, close, stand still) - It is possibile to directly tie three HMI values to PID parameters (Proportional, Integral, Derivative) inside the PID instance DB. But I still can't understand the difference between: - [Input] and [Input_PER] terminals. - [Output] and [Output_PER] terminals Where should I connect my 4-20mA temperature sensor? To [Input] or to [Input_PER] ? Why? Where should I connect my 0-10V regulation valve? To [Output] or to [Output_PER] ? Why? I carefully read the [s71200_system_manual_en-US_en-US.pdf] manual, but didn't find answer to my question. Is there any more detailed documentation, tutorial or example about S7-1200 PID usage? Thank you again.
|
Follow us on