2/14/2012 12:09 PM | |
Posts: 2930 Rating:
|
Dear LOGO! User, Application: A up/Down-Counter is often used to change parameters of a FB via reverencing.The following UDF offers the possibility to increase or decrease the value of a counter depending on pulses (inputs, or similar). The speed change if the inputs is hold. A single impuls increases/decreases the value by 1. UDF name U_D_Count Inputs:UP_Count: increases the value Down_Count: decreases the value Outputs: Value: analog value Dig_Signal: Digital signal if counter value is reached Parameter: TH and TL: if you change this values then you can increase/decrease the counter speed on continues signal at the inputs ON and OFF: Trigger values for the digital output signal. Password of UDF: EDIT Please observe: LOGO! Counts faster then the simulation of the LOGO! Soft comfort Installation of the UDF: 1. Save and unzip the file to a folder on your PC ( remember the folder)
Attention: A UDF only works with LOGO! Soft Comfort V7 AttachmentU_D_Count Var Speed.zip (404 Downloads) |
This contribution was helpful to
2 thankful Users |
2/16/2012 10:01 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hi,
AttachmentFORUM_Tastereingabe_Zähler.zip (384 Downloads) |
==> Meine TAG-Listen: "deut." |
|
Follow us on