(0)| 3/9/2012 1:36 PM | |
|
Joined: 5/26/2007 Last visit: 12/10/2025 Posts: 128 Rating:
|
i got a 6es73141ae020ab0 with a MC (flash eprom 16kB) a cp342-2, a 3211bl00 and a 3221bl00 install. is there a posibility to have a different program in MC and in CPU? when i upload from cpu, in h/w config it show that my di and do as standard module. then i switch off the cpu and turn the key to stop mode, and switch on again. this time i got a different program. i.e: in my first upload i have fc1, then in my second upload i donot have it but i got fc8. some of the fc is same but with different size, when i look inside the fc code, i found the code is almost the same but with the second upload there are some missing line in several network. AttachmentCPU.zip (259 Downloads) |
| 3/9/2012 2:42 PM | |
|
Posts: 1121 Rating:
|
Hi Well do a memeory reset and then download entire program & Hardware and check. Have fun... |
| 3/10/2012 5:03 AM | |
|
Posts: 1064 Rating:
|
What version of step 7 are you using and do you have the current hardware catalog installed ? |
| 3/10/2012 7:19 AM | |
|
Joined: 5/26/2007 Last visit: 12/10/2025 Posts: 128 Rating:
|
step 7 v5.4 yes i have the latest h/w catalog. |
Follow us on