(0)| 12/28/2011 9:28 AM | |
|
Posts: 25 Rating:
|
Hi Ammy, Thanks for your reply I used PCS7 V7.1 SP3 and for Safety used S7 F-System V6.1 BR, Koy |
| 12/28/2011 11:10 AM | |
|
Posts: 2661 Rating:
|
Hi Koy, Have you seen the following FAQ? Why does the error message "Maximum length of code area reached (max. 64 KB)" or "Insufficient main memory" appear when the CFC charts are compiled? Regards |
| 2/24/2012 6:02 AM | |
|
Posts: 133 Rating:
|
Hello I have the exact same problem. I have performed a migration/upgradeof a PCS7 V6.1 projectto PCS7 V7.1 SP3. I have compiled the AS (Charts) without any error. As soon as I download to the PLC I get the error stating that the DB's are out of range. I have attached a screen shot of the starting DB Address area. 1. Is there a way to start generating DB's from DB100 for example so that when the compile is complete the higest DB will be smaller that DB8191? 2. Is there a way to re organize the DB's so that they can automatically fill in the next available DB number so that there are no gaps in between DB numbers? 3. I heard that there is a compress function. How do I access this function? Do I have to be online in order to do the compress? I am glad that I am not the only one experiencing this problem. Thank you kindly AttachmentMaximum length of DB code area.pdf (106 Downloads) |
Follow us on