(0)| 3/24/2012 6:41 AM | |
|
Joined: 9/8/2010 Last visit: 8/21/2025 Posts: 30 Rating:
|
i am working on a 300R configuration with 315-2DP.Basically i have made system healthy with redundancy blocks only(Attached file).After that i have downloaded All DBs in the system and defined DB Number and lenght in the OB100, and Slave CPU changed to STOP mode.Diagnostic buffer message is area lenght error when writing/reading.No instant blocks are yet downloaded.Again if i define db lenght to 0 without deleting DBs, both cpu operate in RUN mode. PLease help me.
AttachmentPOWERCON_ALL_IM_CONFOK.zip (251 Downloads) |
| 3/26/2012 4:28 PM | |
|
Posts: 47 Rating:
|
DB which be to copy must have long >= 2 bytes! |
Follow us on