(0)| 3/16/2012 3:57 PM | |
|
Posts: 2 Rating:
|
Hi, I hope someone can help me further. I am looking for a module that can read an s0 pulse from a kWh meters ( PRO1D ). Its for a s7-300 CPU Some specs. Nom. current 5 A Implementing Single-phase AC Max. flow. 32 A Nom. (measuring) voltage 230 V Nom. (measurement-) operating frequency 45 t / m 55 Hz Pulse output 2000 pulses per kWh, 0.5 Wh / imp. |
Last edited by: msikkema at: 3/16/2012 3:58 PM |
|
Follow us on