(0)| 4/5/2012 9:20 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Question 1) After giving 24V supply, is there any Light on Profibus Module? Red/orange or Green? 2) What do u mean by Adapter? Are you trying to Upload Parameters from Drive to PC? IF yes, thenn what do you mean by this adapter? Are you using Drive-PC kit for MM series drives? Try to insert BOP on Module and check whether you are able to see parameters or Not If Not, then Most chances are, you have not mounted this Profibus Module properly Have a look at following FAQs, that will be useful for you The display on my BOP shows "- - - - -". What could cause this? Micromaster 4 -- Commissioning and operation -- Using STARTER The Profibus unit fitted to the MM4 shows a red or orange light. What can cause this? What is important when setting up an MM4 with a Profibus module? How do I set up my MM4 with Starter or DriveMonitor? Regards, Devesh Vithani |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
| 4/6/2012 10:27 AM | |
|
Posts: 29 Rating:
|
Dear Vithani, Thank you for your reply. The adapter that I mentrioned is 6ES7972-0CB20-0XA0 SIMATIC S7, PC ADAPTER USB . Profibus module is connected to MM420, the orange LED blinks. I connected "adapter" into profibus module, and it doesn't turn on LEDs. Then I connected 24VDC to profibus module, again "adapter" doesn't turn on. |
Last edited by: xhnr at: 4/6/2012 10:28 AM |
|
| 4/6/2012 10:48 AM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello, The mentioned adapter will not work with MM4. You have to use6SE6400-1PC00-0AA0. And also, have a look on this helpful FAQ: Hope this helps. |
|
Ayman Elotaify |
|
| 4/6/2012 3:51 PM | |
|
Posts: 29 Rating:
|
Dear Elotaify, Is it possible to download program through PC -> PLC -> MM420, or I must have 6SE6400-1PC00-0AA0 for downloading program into MM420. Thanks. |
| 4/6/2012 9:02 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Yes you can do it by PC-PLC-MM420 but you need to make routing in your S7 Project and I think your Profibus module should have green LED On means Communication with PLC Have a look at following FAQ for how to Route http://support.automation.siemens.com/WW/view/en/23432199 http://support.automation.siemens.com/WW/view/en/22794082 Regards, Devesh |
Last edited by: Vithani at: 4/6/2012 9:05 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on