(0)| 4/24/2012 6:40 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Well I suggest go for Sinamics instead of MM440 Now regarding your question, yes you can definately read the speed information of the Motor in S7 block. You can use PZD data received from drive or you can read Parameter directly using PKW If you want to know real speed, you have to use Encoder and you will get Encoder speed as feedback otherwise you can use feedback of calculated speed Please refer following FAQ How do I read / write parameters using PROFIBUS on the MICROMASTER 4 and CU240S/D DP/DP-F and PROFINET on the CU240S/D PN/PN-F? Regards Devesh |
Last edited by: Vithani at: 4/24/2012 6:44 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on