(0)| 5/7/2012 5:22 PM | |
|
Joined: 9/28/2005 Last visit: 12/9/2025 Posts: 2957 Rating:
|
Hi, Did you make connection tests on the same computer ? So far as I know there should be no difference at all between those two software versions. There is only restrictions of using it with Micro/WIN: Functional Restriction when using the CP 5711 with MicroWIN Also you could try to update boot loader of your module if its not most recent: Update boot loader for CP 5711 Also it would be good idea to check compatibility with the operating system: Which SIMATIC NET PROFIBUS PC CP is compatible with which Microsoft Windows operating system? |
|
Best regards, |
|
Follow us on