5/7/2012 9:19 AM | |
Posts: 2 Rating:
|
Dear All We are facing some problem in BLM (MLFB-6sl3130-1te31-0aa0, SL no S-T BN2034316) while panel power ON time any of BLM tripping with DC link over voltage ,total 5BLM for5 simotion controller.All BLM getting incoming supply from same source which is 440 v approx. This is facing onlywhile power on time,no other command preset at that time.All simotions are in profinet communication with s7 400 PLC. Any comments regards same subject willbe helpful for us. AttachmentBLM tripping with over voltage.zip (200 Downloads) |
5/8/2012 7:38 AM | |
Joined: 4/30/2012 Last visit: 2/26/2025 Posts: 55 Rating:
|
Hi smijo pls check r297 parameter. If your line voltage is above 435V then change P210 to 415V. regards, maddy |
5/10/2012 4:45 PM | |
Joined: 3/3/2008 Last visit: 4/9/2025 Posts: 333 Rating:
|
HI when does your problem appear ? when the axes is ramping up/down? can you explain in brief regards ram |
Follow us on