(0)| 5/18/2012 6:22 PM | |
|
Joined: 9/24/2011 Last visit: 12/17/2025 Posts: 13 Rating:
|
Dear colleagues, Currently i make project with S7224xp (Microwin SP9) and TP177B (wincc/advanced). In input output fields using memory area V. In example VW100. In the program this variable it was used divided and compared with another one. So it is not possible that this was overwritten by another. From Microwin i can easily change value of it. To change in HMI this i use I/O field. If i use it for output - works perfect. But input-output or input - does not - value remains. Aquisition mode - Cyclic continuous Any ideas?! Attachmentsample.zip (265 Downloads) |
|
Ramunas Labonas |
|
Follow us on