(0)| 6/20/2012 6:41 AM | |
|
Posts: 28 Rating:
|
What should be the P1300 for a gas compressor commssioning. Its urgent.plz help Arijit |
| 6/20/2012 7:50 AM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
I guess you should set P1300=1 and P205=0 I have seperated some pages from Operating Instruction and Parameter List Manuals Please refer them for more help Regards Devesh Vithani Attachment440.zip (162 Downloads) |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
| 6/20/2012 10:38 AM | |
|
Posts: 28 Rating:
|
Thank Vithani for the reply. |
| 6/20/2012 8:17 PM | |
|
Joined: 6/4/2008 Last visit: 11/25/2025 Posts: 1521 Rating:
|
Hi, a quick read of theOPERATING INSTRUCTIONSreveals that F0003 is an undervoltage Fault Can you confirm that 415VAC is present on all supply phases, and that you have the correct DC Link voltage present (Approx Vin * 1.35) Are you using a contactor inline with the supply, and is this being controlled correctly? Regards, Graeme
|
| 6/22/2012 12:55 PM | |
|
Posts: 112 Rating:
|
dear arijit please check the input voltage settings at the p210 and input voltages to the drive at 3 phase |
Follow us on