(0)| 8/2/2012 11:27 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, 1. Cables which are 'good' for backup transfer are :serial RS232(6ES7 901-1BF00-0XA0),USB(Host-to-Host). In order to build by yourself one of both -Which cables can you use for connecting the PC and the TS adapter? 2. Software - Prosave (restore is possible in the same type of panel only) or WinCC FLex (Uploading only possible, if the Transfer of the current project file from the configuration computer to the operating unit mustbe performed using the Upload option "Enable backtransfer".). Like an option is using MMC. Check it athttp://support.automation.siemens.com/WW/view/en/21084916(Backup and restore operations with MMC on OP77B) Best regards, Hristo Mihalev
|
Last edited by: UMENCHO at: 8/2/2012 11:29 AM |
|
This contribution was helpful to
|
|
| 8/4/2012 8:51 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
I don't know if it will works. At least you can try it. Siemens recommedWhich external storage media can you use with the SIMATIC panels and which memory card interfaces do they have? Best regards, Hristo Mihalev
|
Follow us on