(0)| 7/23/2010 11:03 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello jmasino; You are right, Step 5 V. 7.23 is not released for Windows XP SP3. http://support.automation.siemens.com/WW/view/en/6002243 Here is a Microsoft support FAQ on how to remove SP3: http://support.microsoft.com/kb/950249/en-us http://support.microsoft.com/kb/950249/es(en Espanol) I hope it can help you out. Daniel Chartier |
| 7/24/2010 9:29 AM | |
|
Posts: 8946 Rating:
|
Hello Daniel, but Step5 V7.23 HF1 is running very well under XP SP3, also online - funktions are fine. |
This contribution was helpful to
|
|
| 7/26/2010 2:11 PM | |
|
Joined: 7/13/2009 Last visit: 10/16/2025 Posts: 4 Rating:
|
Hello everyone. The problem of opening step 5 on xp sp3 is solved. [schnippschnapp] New question is splitted to I can not open the project with STEP5 V7.23. Greetings. |
Last edited by: O_Moderator at: 7/27/2010 8:55 AMnew question is transferred to another thread |
|
| 8/7/2012 11:02 AM | |
|
Joined: 9/28/2005 Last visit: 10/24/2024 Posts: 414 Rating:
|
Since 20 oct 2011 STEP5 V7.23 is also compatible with WIN XP PROF SP3. See also http://support.automation.siemens.com/WW/view/en/6002243 |
Last edited by: Smurf at: 8/7/2012 11:02 AMadded link to compatibility chart Smurf |
|
This contribution was helpful to
|
|
Follow us on