8/30/2012 1:56 PM | |
Joined: 10/7/2005 Last visit: 9/26/2025 Posts: 3049 Rating:
|
Hello Mr. Darshan bangali Aretis in principal correct that the NW in your screendump by itself doesn't do anything useful with theTimers. With the benefit of being able to read the German comments though and having programmed Sequencers in similar ways before, here's my take on things: Parts of your FB11 (including NW3) are only executed for one scan when the Sequencer changes from one Step to another. The Timers in NW 3 are then executed with an RLO of 0 which initialises them so they can now be used as the Step timers again (they are ready to detect a rising edge again). In other words, this "trick" of initialisingof an S5 Timer when a Step change occurs, allowsevery Step in this Sequence to(re)use thesame S5 Timer. I am of course partially speculating here as you only suppliedcode snippetsbut I hope this helps anyhow. |
Cheers |
|
Follow us on